No-Code PLC Programming Simplifies Industrial Automation Development
Image Source:
tadamichi/Stock.adobe.com
By Abhishek Jadhav for Mouser Electronics
Published May 29, 2026
Programmable logic controllers (PLCs) are key to industrial automation because they are often designed to support deterministic control of machines and processes. However, they are traditionally programmed in specialized languages, such as ladder logic and structured text, as defined by the IEC 61131-3 standard.[1] These languages introduce challenges in maintainability, reuse, and life-cycle management.
However, in recent years, no-code/low-code (NCLC) programming has emerged to reduce barriers to PLC automation development. NCLC helps make programming more accessible to a wider range of engineers and non-programmers, enabling them to contribute to the development and maintenance of industrial control systems.
These modern no-code platforms provide visual editors, flowchart-style logic builders, and pre-built function blocks that users can connect to create automation sequences. These elements mean that little to no textual programming is required. Users don’t need to write lines of code; instead, they configure logic using an intuitive graphical interface. The tool generates the necessary code or execution logic.
Inside No-Code/Low-Code PLC Tools
NCLC platforms operate as visual integrated development environments (IDEs) that abstract the creation of traditional code. In these environments, the engineers interact with a graphical user interface to define logic flows, configure parameters, and link components.
In traditional workflows, visual design documents—such as piping and instrumentation diagrams or mechanical computer-aided design (CAD) models—are static blueprints. These are separated from the dynamic control logic (ladder logic) that stays in the PLC. However, in some modern no-code environments, the visual model can act as an executable specification or generate the underlying control logic.
This approach aligns with model-driven development (MDD), where graphical models are used to generate or configure executable control logic rather than manually writing it. Such programming environments facilitate the development of modular systems in which components such as specific motor controllers, heater loops, or communication drivers can be repurposed.
In addition, the NCLC programming paradigm supports embedded governance, meaning the logic is developed from pre-validated blocks that govern security and access control policies. This paradigm contrasts with conventional coding, where compliance checks are conducted through retrospective code reviews.
The source of truth is often the vendor project representation (i.e., a project database with IEC 61131-3 artifacts and configuration). Some tools can export PLCopen XML or generate structured text.
While NCLC programming protects users from syntax errors during the design phase, the underlying architecture still relies on the compilation and execution of standard code. This creates technical debt, which refers to the future costs, effort, and operational risks arising from suboptimal decisions made during the design, programming, or commissioning phase. Examples include poorly structured control logic, hard-coded parameters, and inconsistent naming conventions.
Even in no-code environments, the generated code must be maintained, patched, and optimized over the system’s life cycle. If the platform’s abstraction leaks, users may need to intervene at the code or configuration level. At that point, previously hidden technical debt can surface.
Strategic Benefits of NCLC PLC Programming
NCLC tools offer a range of advantages for industrial automation:
Lower Skill Barrier
By eliminating the need to learn complex programming languages, no-code PLC platforms make industrial automation development more accessible to engineers and domain experts without extensive programming backgrounds. Drag-and-drop interfaces enable control and process engineers to contribute to the creation of automation logic, helping to bridge the skill gap in manufacturing.
Faster Development
Visual programming and pre-built function blocks significantly accelerate development. Engineers can configure sequences much faster than writing code from scratch, which helps shorten project cycles and speed equipment commissioning. Users can even make changes to the logic on the fly by rearranging blocks or adjusting parameters, which promotes rapid iteration. Overall, NCLC programming reduces time-to-deployment when compared to traditional coding techniques.
Reduced Errors
Since NCLC programming virtually eliminates written code, it eliminates certain classes of syntax errors or programming mistakes, such as misplaced instructions. Many modern NCLC tools perform validation checks on the logic as it is built. These tools also include integrated debugging and monitoring tools that streamline troubleshooting. For example, users can watch real-time variable values, set breakpoints, or insert debug blocks into the logic.
Code Flexibility
While NCLC platforms require minimal coding, many platforms support optional scripting (e.g., Python or JavaScript in edge automation environments) or code extensions to meet custom requirements. Optional scripting offers flexibility to handle edge use cases while enabling users to use visual tools to do most of the coding work. In addition, the visual nature of the logic improves maintainability for teams, as new engineers might be able to follow the flowchart-like diagram more easily than they can read complex code.
Limitations of NCLC PLC Programming
Despite their advantages, NCLC PLC programming tools impose important limitations compared with the full control afforded by traditional programming techniques.
Performance
PLCs are used for deterministic tasks that involve scanning inputs and updating outputs every few milliseconds. A drag-and-drop programming environment can introduce runtime abstraction overhead or execute outside the PLC’s deterministic real-time task. For simple sequences or high-level logic, like data handling or supervisory control, this is usually sufficient.
However, for fast control loops or timing-critical operations, NCLC tools may not be reliable enough to achieve the required determinism or low latency. Best practices are emerging for the NCLC logic to execute on an edge runtime or a supervisory layer alongside the PLC.
Complex Logic
NCLC platforms perform exceptionally well on common, straightforward tasks, but they can struggle with highly specialized control requirements. The available control blocks and templates may not cover all scenarios. Traditional PLC programming gives experts greater control over custom logic, timing, and platform-specific features within the PLC’s real-time and vendor-defined limits. NCLC programming may lead to oversimplification of complex processes.
For example, a highly customized motion-control sequence or an uncommon communication protocol may not be supported by a given low-code tool. Traditional coding offers a level of granularity and control for complex applications that no-code tools may not match.
Transparency
While modern NCLC platforms advertise improved debugging, the transparency of execution behavior may be reduced when compared to written code. In a traditional environment, an engineer can inspect the code to trace a problem or understand the execution order. In NCLC programming, the execution is managed by the platform’s engine, and complex interactions might be harder to trace if they are not visually obvious.
For instance, if an unexpected interaction occurs between two drag-and-drop blocks, a developer may find it challenging to diagnose. Maintaining logical rigor can be challenging as visual workflows grow; a large, poorly structured flowchart can be as difficult to follow as written code.
Conclusion
As industrial automation continues to evolve, NCLC tools will coexist with traditional PLC programming. Each approach is built for different needs: NCLC platforms offer speed, accessibility, and easy integration, while traditional coding provides fine-grained control, performance, and assurance needed for complex tasks.
In the near future, many automation architectures may adopt a hybrid model. For instance, a machine’s basic sequencing might run in standard PLC logic, while safety functions simultaneously run on a safety-rated controller (i.e., safety PLC or safety relay) using certified safety programming and validated procedures, and a no-code tool handles coordination between machines, data logging, and optimization tasks. Organizations that strike the right balance will likely see the greatest benefits.
Sources
[1] https://webstore.iec.ch/en/publication/68533
Author Bio
Abhishek Jadhav received his M.S. in Electrical and Computer Engineering and began his career as a technical writer. He has over five years of experience working as a freelance technical writer, with key interests in power electronics and embedded systems. His work has appeared in EE Times, embedded.com, and Power Electronics News, among others.